Kinetis K27 Absolute maximum rating voltage of USB1_VBUS pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K27 Absolute maximum rating voltage of USB1_VBUS pin

Jump to solution
1,075 Views
masahirokiniwa
Contributor IV

Hi,

Could you tell me the absolute maximum rating voltage of USB1_VBUS pin on Kinetis K27?

I see its tolerant  voltage is 5V in data sheet P.59. But I couldn't find its absolute maximum rating.

How voltage can I applied to it?

Best regards,

M.KIniwa

Labels (1)
0 Kudos
Reply
1 Solution
962 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K27 product is using the same High speed USB module with K26 product.

Customer could refer K26 datasheet about USB1_VBUS Max. rating:

pastedImage_1.png

pastedImage_2.png

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
963 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

K27 product is using the same High speed USB module with K26 product.

Customer could refer K26 datasheet about USB1_VBUS Max. rating:

pastedImage_1.png

pastedImage_2.png

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply