Kinetis K Series: When power is not supplied to VDD and VDDA, is it possible to apply 5V to any pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K Series: When power is not supplied to VDD and VDDA, is it possible to apply 5V to any pin?

Jump to solution
1,058 Views
yasushihasegawa
Contributor III

Dear Kinetis Community Team,

Customer is considering using the Kinetis E series.

He is reading the following data sheet of the Kinetis E series.
http://www.nxp.com/docs/en/data-sheet/MKE02P64M40SF0.pdf


The absolute rating of VIN is (Vdd + 0.3) V in "Table 2. Voltage and current operating ratings" in "4.4 Voltage and current operating ratings" on page 7 of the data sheet.
However, when looking at "Table 3. DC characteristics" in "5.1.1 DC characteristics" on page 8 of the data sheet,
Symbol " IIC (DC injection current)" is described as " VIN < VSS, VIN > VDD" , And the following values are rated:
- Single pin limit: min -2 mA, max 2 mA
- Total MCU limit, includes sum of all stressed pins: min -5 mA, max 25 mA

[Customer's Requirement]
Customer wants to apply 5V to the analog pin before supplying power to VDD and VDDA.

[Question]
Is it possible to satisfy Customer's Requirement by following the above ”IIC (DC injection current)" rating?


Best Regards,
Yasushi Hasegawa

0 Kudos
Reply
1 Solution
919 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Yasushi,


It's ok for KE to apply 5V to the analog pin before supplying power to VDD and VDDA (should be 5V too), while the current is limited within the DC injection current ranges.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
920 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Yasushi,


It's ok for KE to apply 5V to the analog pin before supplying power to VDD and VDDA (should be 5V too), while the current is limited within the DC injection current ranges.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
919 Views
yasushihasegawa
Contributor III

Dear Robin-san,

Thanks for a good reply. 

Best Regards,

Yasushi Hasegawa

0 Kudos
Reply