Kinetis DMA sources/slot assignments

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis DMA sources/slot assignments

ソリューションへジャンプ
2,305件の閲覧回数
richyankee
Contributor II

For DMA - the DMAMUX  needs to have the peripheral slot (DMAMUX_CHCFGn) in the channel source of this register, Isee from a couple of examples on the forum that these are defined (in some include file), but I cannot find the file that contains these definitions.

 

Using IAR, K60 devkit (tower). The user guides and reference manuals say that the peripheral slots are defined in the 'device's Chip Configuration details'. Okay, I have the sub family ref manual, and the peripheral module quick ref.

 

I have the whole MQX developmentn tree and can't find the peripheral slots defined there (maybe I just don't know teh magic words to search for: like peripheral, slot, mux assignment etc.)

 

This is probably easy for somebody who has already set up a dma.

 

Thanks.

 

Rich

 

0 件の賞賛
返信
1 解決策
1,186件の閲覧回数
comsosysarch
Contributor III

https://community.freescale.com/thread/94844

 

K60 Sub-Family Reference Manual, Rev. 6, Nov 2011

pp 92-94

3.3.9.1 DMA MUX request sources

Table 3-24. DMA request sources - MUX 0

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,187件の閲覧回数
comsosysarch
Contributor III

https://community.freescale.com/thread/94844

 

K60 Sub-Family Reference Manual, Rev. 6, Nov 2011

pp 92-94

3.3.9.1 DMA MUX request sources

Table 3-24. DMA request sources - MUX 0

 

0 件の賞賛
返信