KW36 PMC demo?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36 PMC demo?

722件の閲覧回数
jictannu
Contributor III

I want to use low-voltage detect in KW36. I find the api in fsl_pmc.h and fsl_pmc.c, are there any demo or documentation?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

639件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Mo Xinyou, I hope you're doing well!

 

There's some documentation related to LVD in the KW36Z's reference manual, it can be found in chapter 7.2.2.2, and it offers some descriptions about the registers related to this functionality.

 

Additionally, AN4503 has some additional information about the low power modes in Kinetis MCUs, as well as some information about extra features like Low-Power detection.

 

And there's also a section in the Wireless Connectivity Framework User Manual which describes the macros that can be changed to enable LVD on BLE SDK examples. This information can be found in chapter 3.15, and the document itself is included in the SDK archive, in the following path:

 

<…\SDK_2.2.2_FRDM-KW36 - MCUXpresso\docs\wireless\Common\Connectivity Framework Reference Manual.pdf>

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛
返信