KW20 开发zigbee网络 // Development ZigBee Network

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW20 开发zigbee网络 // Development ZigBee Network

ソリューションへジャンプ
2,619件の閲覧回数
thoomanwang
Contributor V

协议库在哪里?

难道是freescale还没公布?

//

Where can I find the protocol library?

Has it been released yet?

Message was edited by: Monica Arvizu

タグ(1)
1 解決策
2,378件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Thooman

Up to now, the zigbee based KW20 protocol library has not yet announced.

Best Regards

Paul

Message was edited by: Monica Arvizu

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,378件の閲覧回数
AlanCollins
Contributor V

Hello Thooman Wang,

The KW20 SW package is now released. Please refer to the following webpage:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT&...

2,378件の閲覧回数
rabbit
Contributor III

I downloaded BeetKit 3.0.1, export a KW2X solution to CW10.4 project, it pass the compiler, but I haven't got the hardware, so I can't do debugging.

We have full license Code Warrior, but no license for IAR.

My question: Can I use Code Warrior to develop KW2X MCU?

Regards

0 件の賞賛
返信
2,378件の閲覧回数
AlanCollins
Contributor V

MKW2x is only supported by IAR IDE.

However MKW2x is a system in package with a K22 MCU + Radio. Then you could use CodeWarrior targeting K22 MCU. The thing is you are on your own, becuase FSL only supports IAR IDE for MKW2x. I strongly recommend you to get IAR. Makes things easier.


Hope this helps. 

0 件の賞賛
返信
2,378件の閲覧回数
thoomanwang
Contributor V

Thank you !
I have downloaded beekit 3.01, is now being tested

0 件の賞賛
返信
2,379件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Thooman

Up to now, the zigbee based KW20 protocol library has not yet announced.

Best Regards

Paul

Message was edited by: Monica Arvizu

0 件の賞賛
返信
2,378件の閲覧回数
thoomanwang
Contributor V

The zigbee protocol library for KW20 about what time can be released ?

There is also a problem , Freescale 's Zigbee system with TI's systems, what the advantages and disadvantages ?

0 件の賞賛
返信