KV58F220M work on 237.5MHz generate great heat. Is It Normal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV58F220M work on 237.5MHz generate great heat. Is It Normal?

446件の閲覧回数
shuangli
Contributor I

Hi,

 

I am testing KV58 minimum system for now. And have the following questions:

I make a kv58 minimum system board refernce TWR-KV58F220M-SCH.pdf, But it generate great heat when I make it work on 237.5MHz.  Is It Normal?

Thanks,
MC Zhu
ラベル(1)
0 件の賞賛
返信
1 返信

344件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, LiShuang,

Pls check the mask of KV58 which you are using, for example, on my TWR-KV58F220M board, the chip PKV58F1M0VLQ22 is used, the last number "22" is is the chip rated frequency, in other words, it can only run in 220mHz rather than 240MHz. If the last two number is "24", which means that the chip can run in 240mhz.

Pls change the MCG so that it can run in 220MHz instead of 240mhz.

Hope it can help you

BR

Xiangjun rong

0 件の賞賛
返信