Hi all,
I'm using board HVP-KV46F150M, with KV46 on it.
KV46 is clocked with external crystal @ 8 MHz, with load capacitors @ 10pF.
I would like to set up system & core clocks to 100 MHz, which is the maximum in RUN mode, according to datasheet.
However, I can't find a configuration matching this requirement when using MCUXpresso Clock Tool.
The reason is that the PLL output frequency must be in range 220 MHz - 480 MHz, and the only way I found to get 100MHz on system/core clock is to have PLL output @ 200 MHz (see attached capture)
Any idea ?
Thanks !
Pierre
已解决! 转到解答。
Hello Pierre,
- It seems if the external crystal is 8Mhz, the PEE mode can not generate core clock with 100MHZ.
From the datasheet we can see the PLL output range is 110MHZ - 240MHZ,
so the range of PLL on Clock configure tool is 220 - 480 , it can't choose 200MHZ.
- You can increase the external crystal, for example 16MHZ:
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Pierre,
- It seems if the external crystal is 8Mhz, the PEE mode can not generate core clock with 100MHZ.
From the datasheet we can see the PLL output range is 110MHZ - 240MHZ,
so the range of PLL on Clock configure tool is 220 - 480 , it can't choose 200MHZ.
- You can increase the external crystal, for example 16MHZ:
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------