KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KV46 : How to get a system/core clock @ 100MHz with 8 MHz crystal

跳至解决方案
4,597 次查看
frq04646
NXP Employee
NXP Employee

Hi all,

I'm using board HVP-KV46F150M, with KV46 on it.

KV46 is clocked with external crystal @ 8 MHz, with load capacitors @ 10pF.

I would like to set up system & core clocks to 100 MHz, which is the maximum in RUN mode, according to datasheet.

However, I can't find a configuration matching this requirement when using MCUXpresso Clock Tool.

The reason is that the PLL output frequency must be in range 220 MHz - 480 MHz, and the only way I found to get 100MHz on system/core clock is to have PLL output @ 200 MHz (see attached capture)

Any idea ?

Thanks !

Pierre

标签 (1)
标记 (1)
1 解答
4,325 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

- It seems if the external crystal is 8Mhz, the PEE mode can not generate core clock with 100MHZ.

From the datasheet we can see the PLL output range is 110MHZ - 240MHZ,

pastedImage_1.png

so the range of PLL on Clock configure tool is 220 - 480 , it can't choose 200MHZ.

- You can increase the external crystal, for example 16MHZ:

pastedImage_2.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
4,326 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Pierre,

- It seems if the external crystal is 8Mhz, the PEE mode can not generate core clock with 100MHZ.

From the datasheet we can see the PLL output range is 110MHZ - 240MHZ,

pastedImage_1.png

so the range of PLL on Clock configure tool is 220 - 480 , it can't choose 200MHZ.

- You can increase the external crystal, for example 16MHZ:

pastedImage_2.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,325 次查看
frq04646
NXP Employee
NXP Employee

Hi Alice,

Thanks for pointing this part of the datasheet out. Answer is clear.

Kind Regards

Pierre