KV30 SPI DMA通道问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV30 SPI DMA通道问题

1,125 Views
Zhang_123
Contributor II

Zhang_123_0-1695729170338.png

在上面的图片中,SPI的例程如果想使用DMA两通道的仅适用于支持GSAKET功能的型号,不支持这个GSAKET功能的MCU是无法使用的,可以这么理解么?对于KV30我在手册中没有找到对应部分,请问它可以使用两通道么?如果不支持GSAKET功能,我可以SPI DMA仅用两通道实现么?非常感谢!

Labels (1)
0 Kudos
Reply
1 Reply

1,087 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

这个SPI_PUSHR寄存器可以分开写, 换句话说, 客户在程序中可以初始化一次高16位。

在存储器中可以只存储16bits 或8 bits的数据,而不存高16bits的控制字,然后由DMA将存储器的16bits 或8 bits的数据搬到SPI_PUSHR寄存器低16 bits。

谢谢

XiangJun Rong

xiangjun_rong_0-1695796591334.png

 

0 Kudos
Reply