KSDK 1.3.0 plugin for KDS 3.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KSDK 1.3.0 plugin for KDS 3.0.0

1,014 次查看
Oriol
Contributor I

I'm going to migrate a MK26FN2M0VMD18 project to MK21FN1M0AVMD12, if it's possible with KDS 3.0.0 IDE with KSDK 1.3.0, which is the IDE and libraries used to develop MK26FN2M0VMD18 project.

According 5.2 section of Getting Started with Kinetis SDK (KSDK) v.1.3.pdf document, if I want to create a project an use KSDK, I need to install KSDK 1.3.0 Eclipse Update. Howerver, after trying to install it I get that error:

KSDK 1.3.0 Eclipse Update
Cannot complete the install because one or more required items could not be found.
Software being installed: KSDK 1.3.0 Eclipse Update 1.0.0.b150914 (com.freescale.processorexpert.kinetis-ksdk-1.3.0.sp.feature.group 1.0.0.b150914)

Therefore, when I create a MK21FN1M0AVMD12 I can't select KSDK 1.3.0.

I would like to avoid using MCUXpresso because it needs KSDK version 2.2 or higher, an I'd prefer don't change the KSDK version.

Did anyone have the same problem as me?

Thank you for you replies.

0 项奖励
回复
0 回复数