KSDK 1.3.0 plugin for KDS 3.0.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KSDK 1.3.0 plugin for KDS 3.0.0

945件の閲覧回数
Oriol
Contributor I

I'm going to migrate a MK26FN2M0VMD18 project to MK21FN1M0AVMD12, if it's possible with KDS 3.0.0 IDE with KSDK 1.3.0, which is the IDE and libraries used to develop MK26FN2M0VMD18 project.

According 5.2 section of Getting Started with Kinetis SDK (KSDK) v.1.3.pdf document, if I want to create a project an use KSDK, I need to install KSDK 1.3.0 Eclipse Update. Howerver, after trying to install it I get that error:

KSDK 1.3.0 Eclipse Update
Cannot complete the install because one or more required items could not be found.
Software being installed: KSDK 1.3.0 Eclipse Update 1.0.0.b150914 (com.freescale.processorexpert.kinetis-ksdk-1.3.0.sp.feature.group 1.0.0.b150914)

Therefore, when I create a MK21FN1M0AVMD12 I can't select KSDK 1.3.0.

I would like to avoid using MCUXpresso because it needs KSDK version 2.2 or higher, an I'd prefer don't change the KSDK version.

Did anyone have the same problem as me?

Thank you for you replies.

0 件の賞賛
返信
0 返答(返信)