KL46Z not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL46Z not working

跳至解决方案
2,014 次查看
Ricky1
Contributor I

When i connect the board to the front USB port (i've tried both) the green LED that indicates that the board is working doesn't turn on.
I've been trying turning it on while pressing the reset button and it works, but the LED blinks 8 times repeteadly and supposedly that indicates error.

Also, the board doesn't show up when connecting, only shows up when connecting it in bootmode (only the bootloader appears).

I used a virtual box with windows 7 and tried to update the boot and it doesn't do anything, the problem still persists.

If someone could help me with this i'd really appreciate it, thanks.

0 项奖励
回复
1 解答
1,975 次查看
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,976 次查看
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

0 项奖励
回复
1,973 次查看
Ricky1
Contributor I
You mean the board isn't broken?
I'll see what i can do, thanks.
0 项奖励
回复
1,970 次查看
ErichStyger
Specialist I

No, it is not broken, but older bootloaders on such boards get confused by Win8 or later host OS. Details in the mentioned article.

0 项奖励
回复
1,931 次查看
Ricky1
Contributor I

I've been trying many times but when i copy and paste the BOOTUPDATEAPP and then disconnect and connect, it doesn't start blinking.
It keeps doing the same, if i keep the RESET button pressed before connecting the LED will start blinking like before (8 times and then stopping, not at 1Hz), but if i don't press anything before connecting, the LED won't turn on.

0 项奖励
回复
1,911 次查看
ErichStyger
Specialist I

Are you using a Windows 7 machine (native, not VM)?

0 项奖励
回复
1,966 次查看
Ricky1
Contributor I
Alright then, thank you so much.
0 项奖励
回复