KL43 Troubleshooting: VLL and VCAP Pins NC is okay?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL43 Troubleshooting: VLL and VCAP Pins NC is okay?

1,081 Views
andrewpikul
Contributor I

I have two KL43's on a board, both on the same power rails. One of them doesn't use an SLCD so I left VLL1,2,3 and VCAP NC. Every GPIO is NC (the peripherals are not soldered on).

The other KL43 works, the described one doesn't. Same software. The described one responds to UART Programmer with proper Reads/Writes/ACKs.

Any ideas? 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

911 Views
soledad
NXP Employee
NXP Employee

Hi,

VCAP pins cannot be floted, or NC,  it is a must that you need to add, a ceramic Capacitor of 0.1uF, since this is a charge pump from the input supply to the internal regulated output, if you do not provide energy the device it is never going to power up.

I hope this helps,


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply