I am trying to move a project between laptops.
They should have identical environments, but the project will not compile at the destination.
From the build console output I can tell all the files are loaded and checked for consistency. At the linker step something goes wrong:
Building target: project.elf
Invoking: Cross ARM C++ Linker
arm-none-eabi-g++ -mcpu=cortex-m0plus -mthumb -Og -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -ffreestanding -fno-builtin -Wall -g3 -T "../../DaqCommon/MKL27Z128xxx4_flash.ld" -Xlinker --gc-sections -Wl,-Map,"GDX-SND-0T1.map" --specs=nano.specs -mapcs -Xlinker -static -Xlinker -z -Xlinker muldefs -Xlinker --defsym=__usb_ram_size__=0x800 -o "project.elf"...
project.elf section `.flash_config' will not fit in region `m_flash_config'
section .text loaded at [00000410,00012017] overlaps section .flash_config loaded at [00000400,0000041f]
region `m_flash_config' overflowed by 16 bytes
collect2.exe: error: ld returned 1 exit status
I believe this memory section is being built in startup_MKL27Z4.S file with:
.syntax unified
.arch armv6-m
.section .isr_vector, "a"
.align 2
.globl __isr_vector
__isr_vector:
.long __StackTop /* Top of Stack */
… … … … … ...
.long PORTC_PORTD_IRQHandler /* Single interrupt vector for PORTC; PORTD Pin detect*/
.size __isr_vector, . - __isr_vector
/* Flash Configuration */
.section .FlashConfig, "a"
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFFFFFF
.long 0xFFFF31FE
.text
.thumb
/* Reset Handler */
.thumb_func
.align 2
.globl Reset_Handler
.weak Reset_Handler
... ... ...
The code is only trying to populate 16 bytes, as the memory space requires, so why does it overrun by 16 bytes?
What in the environment could cause this to memory space to be built twice?