KL25Z - Wakeup using TSI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL25Z - Wakeup using TSI

跳至解决方案
2,323 次查看
javervalino
Contributor III

Hi All,

Good day!

I'm currently using frdm-kl25z board. I was able to test the sample program for touchpad using TSS. In this example, the board will go to sleep mode after several second when no touch is detected.

You can wake-up the board by touching the right electrode. My question is that, is there a way to wakeup the board by touching any of the 2 (left or right) electrodes?

Thanks in advance.

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,838 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Javer

On the kinetis L you can only scan channel by channel, this is  defined by TSI_DATA[TSICH] , when the MCU goes to low power, the value that is on TSI_DATA[TSICH]  is the only channel that can wake up the device.

Unfortunately there is not possible use two different electrodes to wake up the MCU on Kinetis L

Vicente

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,838 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Javer

Would you please tell me which sample project you use?

Best Regards

Paul

0 项奖励
回复
1,838 次查看
javervalino
Contributor III

Hi Zhe,

I use the provided sourcode by xtrinsic from this link "TSS: Xtrinsic Touch-Sensing Software". Mine is located in this directory "C:\Freescale\Freescale_TSS_3_1\examples\FRDMKLXX_DEMO".

I hope there's a work around for this. :smileyhappy:

Thank you and best regards,

Javer

0 项奖励
回复
1,839 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Javer

On the kinetis L you can only scan channel by channel, this is  defined by TSI_DATA[TSICH] , when the MCU goes to low power, the value that is on TSI_DATA[TSICH]  is the only channel that can wake up the device.

Unfortunately there is not possible use two different electrodes to wake up the MCU on Kinetis L

Vicente

0 项奖励
回复
1,838 次查看
javervalino
Contributor III

Hello Pedro,

Can you give an example how to wake-up using tss in processor expert?

Thanks in advance..

0 项奖励
回复