KL25 documentation - can't figure out sources for DACREF_1, DACREF_2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KL25 documentation - can't figure out sources for DACREF_1, DACREF_2

跳至解决方案
1,933 次查看
Smiffytech
Contributor III

The KL25 Sub-Family Reference manual describes the DAC in Chapter 30.

  • 30.2 - Features - it is stated that Vin can be selected from two reference sources.
  • Block diagram shows DACREF_1, DACREF_2 coming from (somewhere.)
  • 30.5 - Functional description: "see the module introduction for information on the source for DACREF_1 and DACREF_2."
  • Module introduction (30.1) doesn't give any mention - we're back where we started.

Could someone please point me to where these sources are described - or what they are if they aren't.

Thanks!

标记 (2)
0 项奖励
回复
1 解答
1,753 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Matthew

In KL25 reference manual chapter 3.2.2 "Analog reference options", you can find 12-bits DAC has two reference voltages for reference. One is VREFH and the other one is VDDA. If you use manual "KL25P80M48SF0RM", you can find on page 48.

Hope my reply can help you.

Best Regards

Paul

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,753 次查看
Smiffytech
Contributor III

Thanks! Do I need to raise a ticket? The documentation, as it stands, isn't really helpful, and should certainly refer back to 3.2.2, rather than "see the module introduction," (which I interpret as 30.1) where no mention is made at all.

From practical purposes, since I'm actually trying to do something with a Freedom board, I believe these two lines are tied together anyway.

0 项奖励
回复
1,753 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Matthew

It is no need to raise a ticket. Your idea is a good idea. It is a direction we need to improve. Thanks.

Best Regards

Paul

0 项奖励
回复
1,754 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Matthew

In KL25 reference manual chapter 3.2.2 "Analog reference options", you can find 12-bits DAC has two reference voltages for reference. One is VREFH and the other one is VDDA. If you use manual "KL25P80M48SF0RM", you can find on page 48.

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复