KL25 blocked after an errate write on MCG_C2 register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL25 blocked after an errate write on MCG_C2 register

582 Views
alessiopaolucci
Contributor III

I try to do a driver for setting the clock of the kl25 mcu.

I wrote the FBI to FEE transiction function in this way:

uint32_t fbi2fee (uint32_t fext, uint8_t dmx32, uint8_t drst_drs, uint8_t range0, uint8_t frdiv)

{

  uint32_t fout_MCG = 0;

  MCG_C2_REG(regmap) &= ~(MCG_C2_RANGE0_MASK);

  MCG_C2_REG(regmap) = MCG_C2_RANGE0(range0);

  .....

}


I think that the problem comes from the fact that in this state transition I forgot to use a temporary variable to clear the field C2_RANGE0 , since I was using the crystal oscillator at 8MHz, and so range0 must be equal to 1 or 2 and I write 0 in C2_RANGE0 field to clear it.


From the moment of this write on the register C2 I can't connect to the MCU.


Seems that SDA work properly, but I can' t connect my PC to MCU.


Help me! How can I unlock the MCU and this situation?


Best regard

Alessio Paolucci

Labels (1)
0 Kudos
2 Replies

348 Views
jeremyzhou
NXP Employee
NXP Employee

Hi ,

I'd like to suggest that you can refer to this post to unlock your MCU.]

If you have any other questions, please feel free to contact with me.

How to unlock flash for MKL25Z128VLK4
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

348 Views
alessiopaolucci
Contributor III

Thank you for your suggestion!

Have a nice day,

Alessio

0 Kudos