KL04 RM (page 119): NMI_DIS : “1” NMI interrupt reset enabled.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL04 RM (page 119): NMI_DIS : “1” NMI interrupt reset enabled.

498 Views
HeMyFAE
NXP Employee
NXP Employee

Dear Kinetis L ,

KL04 RM (page 119):

http://cache.freescale.com/files/32bit/doc/ref_manual/KL04P48M48SF1RM.pdf?fpsp=1&WT_TYPE=Reference Manuals&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation&Parent_nodeId=1339519439021722350580&Parent_pageType=product               

Can you help me confirm whether the bit definition is correct?

NMI_DIS  :  “1”   NMI interrupt reset enabled.

I think  “1” should be disabled and not enabled.

Please help me verify with the designer.

Thx,

hy

Labels (1)
0 Kudos
2 Replies

230 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Hy,

The FTFA_FOPT config byte is located at flash address 0x40D, which set "1" to enable NMI function in FTFA_FOPT register to make sure 0x40C default value 0xFF make NMI function enabled.

Wish it helps.

B.R.

Ma Hui

0 Kudos

230 Views
al_muir
NXP Employee
NXP Employee

The definition in the reference manual is correct - a "1" means the NMI function is enabled, a "0" means the NMI function is disabled.

0 Kudos