KEAZ64AMLH ADC problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KEAZ64AMLH ADC problem

1,191 次查看
hansonhe
NXP Employee
NXP Employee

Dear,

Problem Description:
We meet below problem for channel AD2 and AD3.
When AD2, AD3 two channel sampling. During the loading test, the AD2 connection wire will fall off, so AD2 pin PTA6 is not connected with other thing, at this situation we sample AD3, and then AD2, it is found that the value of AD2 changes with the change of AD3 value. In addition, if you read the value of the AD2 first and read the value of the AD3, this problem does not exist.
At present, all the boards can repeat the problem. The attachment is the test code and the schematic diagram. Please help see if there is any other special attention to ADC. Thank you.

 

0 项奖励
回复
1 回复

1,054 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Hanson,

Same question in Case 00149224.
Consider the ADC is used to detect keyboard, it does not require very high accuracy.
Please pullup or pulldown a large resistor at ADC pin, it will ensure the ADC value to high or low when the ADC input is floating.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复