KEAZ64 can't enter into stop mode while DIO pin and CLK pin disabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KEAZ64 can't enter into stop mode while DIO pin and CLK pin disabled

2,466 次查看
Wangerxi
Contributor II

As the subject, KEAZ64 enter into stop mode succeed every time, however it doesn't work while DIO pin and CLK pin disabled.

0 项奖励
回复
6 回复数

2,457 次查看
Wangerxi
Contributor II

Hi Robin,

Thanks for your reply, I disable SWD function by config PE and judge based on the measured current.

Wangerxi_0-1636101682882.png

 

BR

Erxi

0 项奖励
回复

2,442 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you tested the project in that discussion? Add that code can still enter STOP mode. 
The hardware that needs to be changed on the development board is also mentioned there.

0 项奖励
回复

2,430 次查看
Wangerxi
Contributor II

Hi Robin

I tested my own board,not development board.

 

0 项奖励
回复

2,423 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

That example does not use other peripherals, just puts the MCU into STOP mode.(So I think you can test it on your custom board)
You need to refer to the points of attention in that discussion and check whether your external circuit has any part that affects power consumption.

Avoid some bad case:

Fig3_internalpullupdowncell.JPG

0 项奖励
回复

2,413 次查看
Wangerxi
Contributor II

Hi Robin,

Thanks for your help, I will check it based on your advice.

0 项奖励
回复

2,462 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Wangerxi,

Did you disable SWD function by cleasr the SWDE of SIM_SOPT0?
SIM_SOPT0 &= ~SIM_SOPT0_SWDE_MASK;


How did you know the MCU didn't enter into stop mode?
If you are judging based on the measured current, then please refer the discussion in how to achieve the KEA128 lowest static current in STOP mode

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复