In my KEAZ64 project , when I reference to a pointer , the MCU will reset .
I have traced the code ,found the value is correct . But once step to the line :
nTblSize = pTSAInfo->tblSize;
the MCU will reset .
Double check the code , NOT found what's wrong.
I tried in KDS and CW 10.7 ,got the same result .
Please help to check it .
I simplify all the code in one file to demo the issue as following:
And also attached the KDS project file.
/*
* Copyright (c) 2015, Freescale Semiconductor, Inc.
* All rights reserved.
*
*/
#include "SKEAZ1284.h"
static int i = 0;
typedef unsigned char FMSTR_U8;
typedef unsigned short FMSTR_U16;
typedef unsigned char *FMSTR_ADDR;
typedef unsigned char FMSTR_BCHR;
typedef unsigned char* FMSTR_BPTR;
typedef unsigned char BOOL;
typedef unsigned char BYTE;
typedef unsigned short WORD;
typedef unsigned long DWORD;
typedef void * LPVOID;
#define NULL 0
typedef struct
{
//feed para
FMSTR_U8 cmd; //command code ,the response is for this cmd
FMSTR_U8 len; // command data len
FMSTR_U8 subitem; // sub imtem
FMSTR_U8 ReadMemEX_Size; // size for readMemEX
FMSTR_ADDR ReadMemEX_Addr; // address for readMemEX
FMSTR_BPTR pData; // point to data IO buffer
//return para
FMSTR_U8 status; //command return status
} MCB_RESP,*pMCB_RESP;
typedef struct
{
WORD tsaFlags;
WORD tblSize;
DWORD tblAddr;
} MCB_RESP_GETTSAINFOEX, * LPMCB_RESP_GETTSAINFOEX;
static FMSTR_BCHR pcm_pCommBuffer[67];
static MCB_RESP FMSTR_CMD_RESP;
static FMSTR_BPTR pcm_pRxBuff;
int main(void)
{
/* Write your code here */
LPMCB_RESP_GETTSAINFOEX pTSAInfo;
pMCB_RESP pCmdResp =NULL;
MCB_RESP ** ppCmdResp;
FMSTR_U16 nTblSize;
pcm_pRxBuff = pcm_pCommBuffer;
*pcm_pRxBuff++ = 0x00;
*pcm_pRxBuff++ = 0x02;
*pcm_pRxBuff++ = 0x01;
*pcm_pRxBuff++ = 0x00;
*pcm_pRxBuff++ = 0x02;
*pcm_pRxBuff++ = 0xEC;
*pcm_pRxBuff++ = 0x92;
*pcm_pRxBuff++ = 0x00;
*pcm_pRxBuff++ = 0x00;
*pcm_pRxBuff++ = 0x7D;
FMSTR_CMD_RESP.pData = pcm_pCommBuffer+1;
ppCmdResp = & pCmdResp;
*ppCmdResp = & FMSTR_CMD_RESP;
pTSAInfo = (LPMCB_RESP_GETTSAINFOEX)(pCmdResp->pData);
nTblSize = pTSAInfo->tblSize; // Run to here, the MCU will reset
/* This for loop should be replaced. By default this loop allows a single stepping. */
for (;;) {
i++;
}
/* Never leave main */
return 0;
}
////////////////////////////////////////////////////////////////////////////////
// EOF
////////////////////////////////////////////////////////////////////////////////
Original Attachment has been moved to: keaz64_t1.zip
解決済! 解決策の投稿を見る。
Hi
The Cortex m0+ (in KEA) can't access unaligned addresses.
Your code is assigning an unaligned address to a struct pointer and so when
nTblSize = pTSAInfo->tblSize; // Run to here, the MCU will reset
is executed it will be trying to read a short word from an unaligned address in RAM.
This is the line that more or less forces the failure:
FMSTR_CMD_RESP.pData = pcm_pCommBuffer + 1;
as pcm_pCommBuffer[] is very probably aligned to start on a long word boundary (but possibly not guaranteed) so you are forcing a misaligned struct pointer.
Cortex m4 will work since it supports misaligned addressing (but is slower in the process).
Therefore it is not a compiler or IDE problem but incorrect code design in a Cortex m0+ environment.
You will need to rework the buffer design to ensure that if you want to access using struct pointers that the byte array memory is suitably (and guaranteed ) aligned. Alternatively you could do
typedef struct
{
unsigned char tsaFlags[2];
unsigned char tblSize[2];
unsigned long tblAddr[4];
} MCB_RESP_GETTSAINFOEX, *LPMCB_RESP_GETTSAINFOEX;
nTblSize = ((pTSAInfo->tblSize[0] << 8) | pTSAInfo->tblSize[1]);
to ensure no access risks but it is a bit fiddly and less efficient (but very safe and unconditionally portable).
Regards
Mark
Professional support for Kinetis: http://www.utasker.com/index.html
Remote desktop one-on-one coaching: http://www.utasker.com/services.html
Getting started to expert videos: https://www.youtube.com/results?search_query=utasker+shorts
Hi
The Cortex m0+ (in KEA) can't access unaligned addresses.
Your code is assigning an unaligned address to a struct pointer and so when
nTblSize = pTSAInfo->tblSize; // Run to here, the MCU will reset
is executed it will be trying to read a short word from an unaligned address in RAM.
This is the line that more or less forces the failure:
FMSTR_CMD_RESP.pData = pcm_pCommBuffer + 1;
as pcm_pCommBuffer[] is very probably aligned to start on a long word boundary (but possibly not guaranteed) so you are forcing a misaligned struct pointer.
Cortex m4 will work since it supports misaligned addressing (but is slower in the process).
Therefore it is not a compiler or IDE problem but incorrect code design in a Cortex m0+ environment.
You will need to rework the buffer design to ensure that if you want to access using struct pointers that the byte array memory is suitably (and guaranteed ) aligned. Alternatively you could do
typedef struct
{
unsigned char tsaFlags[2];
unsigned char tblSize[2];
unsigned long tblAddr[4];
} MCB_RESP_GETTSAINFOEX, *LPMCB_RESP_GETTSAINFOEX;
nTblSize = ((pTSAInfo->tblSize[0] << 8) | pTSAInfo->tblSize[1]);
to ensure no access risks but it is a bit fiddly and less efficient (but very safe and unconditionally portable).
Regards
Mark
Professional support for Kinetis: http://www.utasker.com/index.html
Remote desktop one-on-one coaching: http://www.utasker.com/services.html
Getting started to expert videos: https://www.youtube.com/results?search_query=utasker+shorts