I what to measure the time interval of rising edge of two pulses with CH0 and CH1 of FTM2.
As the figure below,the yellow line and the bule line. FTM2 clock is 40M.
When there is only one blue pulse , I could measure the time interval corretly.
But when there are there blue pulses, I what measure the rising edge of yellow pulse and the first
rising edge of bule pulse, the result is the yellow pulse and the third blue pulse. I can't measure the
the rising edge of yellow pulse and the first rising edge of bule pulse.I have tried to set the filter of CH0
and CH1 with different values,but no work. How to solve this problem?
Can you please provide me your response on the above issues or can we connect over a call for a better demonstration of the issues.
Regards,
Hi cqhcau,
We can continue to discuss in your post. Have you tried disable the input capture once you read the first value of C2V?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I have tried to disable the input capture Isr of CH1(with CHIE) in the Isr handler,but no use.
Do you mean to disable the CH1 capture with DECAPEN,COMBINE,CPWMS,MSnb:Msna ?