Hello All,
I am having issue with TRK-KEA8 BOARD Pull-up Disable
| #define PORT_PTA0 0 |
#define PORT_PTA1 1
#define PORT_PTA2 2
#define PORT_PTA3 3
#define PORT_PTA4 4
#define PORT_PTA5 5
#define PORT_PTA6 6
#define PORT_PTA7 7
#define PORT_PTB0 8
#define PORT_PTB1 9
#define PORT_PTB2 10
#define PORT_PTB3 11
#define PORT_PTB4 12
#define PORT_PTB5 13
#define PORT_PTB6 14
#define PORT_PTB7 15
void main(void)
{
asm("CPSID i"); // Disable Interrupt
ICS_C1|=ICS_C1_IRCLKEN_MASK; /* Enable the internal reference clock*/
ICS_C3= 0x90; /* Reference clock frequency = 39.0625 KHz*/
while(!(ICS_S & ICS_S_LOCK_MASK)); /* Wait for PLL lock, now running at 40 MHz (1024 * 39.0625Khz) */
ICS_C2|=ICS_C2_BDIV(1) ; /*BDIV=2, Bus clock = 20 MHz*/
ICS_S |= ICS_S_LOCK_MASK ; /* Clear Loss of lock sticky bit */
WDOG_CNT = 0x20C5; // write the 1st unlock word
WDOG_CNT = 0x28D9; // write the 2nd unlock word
WDOG_TOVALL = 10; // Write New Word in WDT : 10 x (1 / 1000) = 10 msec but cause of tolerance it's 16msec (Appx. +25 /-35 %)
WDOG_TOVALH = 0;
WDOG_CS2 = 0x01; // Select clock 1Khz ; to select 32 Khz clock we need to Enable in ICS_C1 register internal reference clock enable bit ICS_C1[IRCLKEN]
WDOG_CS1 = 0x80; // Enable WDT : Feed the Dog : Activate the Dog
SIM_SOPT = 0xC; // PTB4 Default to NMI function: PTB4 to Normal GPIO
GPIOA_PDDR = 0xF7F2; // Define PortA (A1-A3) all Pin As Output ; one is Output and Zero is Input
// After POR : Power on Reset The Port Pins are in High Impedance State
GPIOA_PIDR &= ~1 ; // configure PORTA0 pin as GPIO input, must clear PIDR bit
GPIOA_PIDR &= ~2048 ; // configure PORTB3 pin as GPIO input, must clear PIDR bit
// 0 and 11 are Register Bit to clear A0 and B3 refer GPIO Register Bit Assignment Datasheet Table 33-21
GPIOA_PDDR |= 0 << PORT_PTA0 ; // direction is INPUT , PORTA0
GPIOA_PDDR |= 0 << PORT_PTB3;
GPIOA_PDOR = 0x0000; // Initialise the PORTA, PORTB
PORT_PUEL &= 0 << PORT_PTA0 ;
PORT_PUEL |= 1 << PORT_PTA2 ; // Pull Enable on A0(Default Pull-up ENable Cause of programming Pin), A2 and A3 0X0000D
PORT_PUEL |= 1 << PORT_PTA3 ;
PORT_PUEL & = 0 << PORT_PTA2 ; // Disable pull-up
PORT_PUEL &= 0 << PORT_PTA3 ;
}
Problem:
It's a part of my code , i am trying to disable the Individual Pull-Up , as i my case first enabled Pull up on PORTA2 and PORTA3 and then Disabled (just for debugging but in real code Pull-up disable is after 20msec) , it disable both the Pull-Up PORT bits PORTA2 and PORTA3 both at the same time i.e. by first instruction of pull-up disable PORT_PUEL & = 0 << PORT_PTA2 . it's not disabling the individual Bits , instant of that whole Port Pull-up? why?
Info : Both pins are Open Drain pins and having SDA/SCL Structure (Please refer page number 142 OF KEA8 Sub Family Reference manual)
Note: I test it on LED and also seen on Debugging register getting same result as i mentioned above.
Robin
PORT_PUEL &= 0 << PORT_PTA3 ;
is the same as
PORT_PUEL &= 0;
is the same as
PORT_PUEL = 0;
therefore it disables all pull-ups
I think you wanted to write
PORT_PUEL &= ~(1 << PORT_PTA3) ;
Regards
Mark
Kinetis: µTasker Kinetis support
KE: µTasker FRDM-KE02Z support / µTasker FRDM-KE02Z40M support / µTasker FRDM-KE06Z support
For the complete "out-of-the-box" Kinetis experience and faster time to market
Hello Mark,
I need Assembly Instructions set to know the bus cycles for each Assembly instructions for KEA8 controller , please can you tell me where i will find ? It's not given in datasheet :smileysad:
Thanks in Advance.
MFG
Robin
Robin
For information about the core you need to use ARM documentation.
http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0432c/CHDCICDF.html
Regards
Mark
Kinetis: µTasker Kinetis support
KE: µTasker FRDM-KE02Z support / µTasker FRDM-KE02Z40M support / µTasker FRDM-KE06Z support
For the complete "out-of-the-box" Kinetis experience and faster time to market
Thank you Mark :smileyhappy:
Have a nice Day !!!