KEA128 sleep mode wakeup through mscan wakeup interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 sleep mode wakeup through mscan wakeup interrupt

1,185 Views
大大许
Contributor III

Hi ,

I  want to wakeup kea128 through mscan wakeup interrupt.

First I trial mscan wakeup interrupt in mscan sleep mode(SLPRQ = 1 && SLPACK = 1), it can wakeup by wakeup interrupt.

However ,I try to make MSCAN entre sleep mode , setting wakeup interrupt bit and enable bit ,making KEA128 entre Sleep mode through WFI instruct ,I can't wakeup cpu through mscan wakeup interrupt.

Am i ingoring something?

Thanks.

Labels (1)
0 Kudos
Reply
1 Reply

947 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I am not sure if you have slove this issue(Assumed Answered).

The MSCAN(Sleep mode) wake-up interrupt should be able to wakeup KEA128 from sleep(WAIT) mode.

32.4.6 Low-power options.png
It's one of the AWIC stop wakeup source listed in "Table 3-11. AWIC stop wakeup sources".

Table 3-11. AWIC stop wakeup sources.png

Please notice:

32.4.8.4 Wake-up interrupt.PNG

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------