KE1xF SDK FOPT BOOTSRC_SEL definition error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE1xF SDK FOPT BOOTSRC_SEL definition error

733 Views
asapuntz
Contributor I

Rev 4 of MKE18F16.h (SDK 2.8.0) has

#define NV_FOPT_BOOTSRC_SEL_MASK (0xC0U)
#define NV_FOPT_BOOTSRC_SEL_SHIFT (6U)

This doesn't match KE1xF RM 22.3.1 / Table 22-2, which indicates BOOTSRC_SEL is just FOPT[7], and the choice of boot source depends on both FOPT[7] and FOPT[1] (BOOTPIN_OPT), rather than FOPT[7:6]

I would think the definitions above should be changed to 0x80U and 7U, respectively?

It would also be nice to #define NV_FOPT_RSVD (0x70U)

0 Kudos
Reply
1 Reply

722 Views
jay_heng
NXP Employee
NXP Employee

You are right, it should be as below in SDK

#define NV_FOPT_BOOTSRC_SEL1_MASK (0x80U)
#define NV_FOPT_BOOTSRC_SEL1_SHIFT (7U)

#define NV_FOPT_BOOTSRC_SEL0_MASK (0x02U)
#define NV_FOPT_BOOTSRC_SEL0_SHIFT (1U)

FOPT.PNG

0 Kudos
Reply