KE04Z8 - What's in flash between 0x0000 to 0x0400

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KE04Z8 - What's in flash between 0x0000 to 0x0400

Jump to solution
944 Views
IlConte
Contributor IV

Dear all.

I use CW 10.6 and KE04Z8.

I now that in flash between 0x400 to 0x40F there is protection register of cfmprotrom   

The map of default cw project is:

.interrupts     0x00000000       0xc0
                0x00000000                __vector_table = .
                0x00000000                . = ALIGN (0x4)
 *(.vectortable)
 .vectortable   0x00000000       0xc0 ./Project_Settings/Startup_Code/kinetis_sysinit.o
                0x00000000                InterruptVector
                0x000000c0                . = ALIGN (0x4)

.cfmprotect     0x00000400        0x0
                0x00000400                . = ALIGN (0x4)
 *(.cfmconfig)
                0x00000400                . = ALIGN (0x4)

.text           0x00000800      0x268
                0x00000800                . = ALIGN (0x4)
 *(.text)
 *(.text*)

I have moves the start from 0x800 to 0x410 but . .  How can i use the zone fron 0x0010 (after vector) to 0x0400 ?

My question is : What there is from 0x0010 to 0x0400 ?

How can i use it ?

Thanks

Stefano

0 Kudos
Reply
1 Solution
865 Views
mjbcswitzerland
Specialist V

Hi Stefano

If you locate interrupt vectors in Flash they will occupy from 0x00000010 to 0x0000007a (the KE04 has 28 interrupt vectors). Between here and 0x400 there is nothing and so can be used to locate const variables, or code to if you wish.

If you locate interrupt vectors to SRAM (and don't have a copy of them in the default vector area of flash) the area from 0x00000010 to 0x0x000003ff will be free for such usage too.

Most likely, due to the very small SRAM size in a KE04Z8 (1k), you will be using fixed vectors in Flash.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
KE04: http://www.utasker.com/kinetis/FRDM-KE04Z.html

View solution in original post

1 Reply
866 Views
mjbcswitzerland
Specialist V

Hi Stefano

If you locate interrupt vectors in Flash they will occupy from 0x00000010 to 0x0000007a (the KE04 has 28 interrupt vectors). Between here and 0x400 there is nothing and so can be used to locate const variables, or code to if you wish.

If you locate interrupt vectors to SRAM (and don't have a copy of them in the default vector area of flash) the area from 0x00000010 to 0x0x000003ff will be free for such usage too.

Most likely, due to the very small SRAM size in a KE04Z8 (1k), you will be using fixed vectors in Flash.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
KE04: http://www.utasker.com/kinetis/FRDM-KE04Z.html