KE02 pinout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KE02 pinout

跳至解决方案
1,661 次查看
dporada
Contributor III

I am laying out a prototype board for the MKE02Z64VQH2 (64 pin package).  I want to use both SPIs, but the reference manual seems to have an error.  SPI0_MOSI is shown on pin 31 and 59. SPI0_SCK is shown on pins 32 and 60.  I do not see a SPI1_SCK, SPI1_MOSI.

Any ideas of the correct pinout?

标签 (1)
0 项奖励
回复
1 解答
1,461 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Donald,

  In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.

-Anthony

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,462 次查看
anthony_huereca
NXP Employee
NXP Employee

Hi Donald,

  In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.

-Anthony

0 项奖励
回复
1,461 次查看
dporada
Contributor III

Oops, you are correct.

I was looking at Alt 2 where the rest of the SPI pins were configured, not at Alt 3.

Thank you,

Don Porada

0 项奖励
回复