I am needing to check/set the configuration for the POR voltage level and the LVD levels. I see nn the Component Inspector where the LVD values can be set. However, it shows the LVD voltage threshold can be set to either Low or High. (I assume the word "treshold" in the KDS tools really means "Threshold"?). However, where can I find the exact voltage values for the settings of High and Low? Also, is there an entry somewhere in the tools for setting the Vpor value as well?
Thanks,
Bill
Hi Bill,
You can check this information in the datasheet:
http://cache.nxp.com/files/microcontrollers/doc/data_sheet/MKE02P64M40SF0.pdf
There is the Table 4 about LVD and POR levels. VPOR voltage is not configurable:
Best regards,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------