KBI pinout in kinetis M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KBI pinout in kinetis M

1,119件の閲覧回数
andresbaena
Contributor II

hello

the kinetis family m, not have KBI interrupt.

thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

911件の閲覧回数
PatriciaTeran
Contributor III

hi, Andres

The family M does not have it by the name of KBI interrupt, but you can use GPIO as an interrupt. If you go to Chapter 11 of the Reference Manual, you can find more information about how to configure it, section 11.5.1 describes the Pin Control Register, where you can configure the pin to generate the interrupt request

You can also refer to eGPIO which is described in section 3.10.1

Hope it helps

Regards

Patricia

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信