KBI Interrupt on KE02

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KBI Interrupt on KE02

Jump to solution
1,912 Views
lmg
Contributor III

I am attempting to use the KBI0, Pin 1 Interrupt on a KE02Z processor.

I am using Kinetis Design Studio 3.2.0 with Processor Expert version shown below:

pastedImage_1.png

The KBI Processor Expert (Sync_Int:init_KBI) component looks like this:

pastedImage_2.png

and appears to be a bit incomplete.

I've modified/added-to the automatically-generated code and here's what I have so far:

/*
** ===================================================================
** Method : Sync_Int_Init (component Init_KBI)
** Description :
** This method initializes registers of the KBI module
** according to the Peripheral Initialization settings.
** Call this method in user code to initialize the module. By
** default, the method is called by PE automatically; see "Call
** Init method" property of the component for more details.
** Parameters : None
** Returns : Nothing
** ===================================================================
*/
void Sync_Int_Init(void)
{
// Connect system clock to KBI0 module (not well documented)
SIM_SCGC |= SIM_SCGC_KBI0_MASK;
/* KBI0_SC: ??=0,??=0,??=0,??=0,KBF=0,KBACK=0,KBIE=0,KBMOD=0 */
KBI0_SC = 0x00;
/* KBI0_ES: KBEDG=2 */
KBI0_ES = KBI_ES_KBEDG(0x02);
/* KBI0_PE: KBIPE=2 */
KBI0_PE = KBI_PE_KBIPE(0x02);
/* KBI0_SC: KBACK=1 */
KBI0_SC |= KBI_SC_KBACK_MASK;
/* KBI0_SC: KBIE=1 */
KBI0_SC |= KBI_SC_KBIE_MASK;
}

/*
** ###################################################################
**
** The interrupt service routine(s) must be implemented
** by user in one of the following user modules.
**
** If the "Generate ISR" option is enabled, Processor Expert generates
** ISR templates in the CPU event module.
**
** User modules:
** main.c
** Events.c
**
** ###################################################################
** */
PE_ISR(Sync_Interrupt)
{

/* KBI0_SC: KBIE=1 */
KBI0_SC |= KBI_SC_KBACK_MASK;

... <my code here>

}

I can download the code and KBI seems to initialize ok, but the ISR is never called.

I found this post:

Making a KBI Library... 

which (at the end of the reply) references NVIC_ICER and NVIC_IPER6. I see documentation on the second register - just a place to set the interrupt priority. But what is NVIC_ICER? I don't see that even mentioned in the reference manual. Is there a bit in that register that turns on the KBI interrupt?

Thanks in advance for any insight you can provide.

~LMG

0 Kudos
Reply
1 Solution
1,766 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Here is the NVIC register summary, see NVIC_ISER and NVIC_ICER:

NVIC ISER ICER.png

The Interrupt vector assignments of KBI0 in KE02 are same as KE04, you can use the codes in that post.

Interrupt vector assignments.png

From your codes, rising edge is configured for this pin. Did you enable internal pull-down or put external pull-down for KBI0 pin1?

Here the "deasserted logic levels" is 0v for your configuration.Edge-only sensitivity.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
1,767 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Here is the NVIC register summary, see NVIC_ISER and NVIC_ICER:

NVIC ISER ICER.png

The Interrupt vector assignments of KBI0 in KE02 are same as KE04, you can use the codes in that post.

Interrupt vector assignments.png

From your codes, rising edge is configured for this pin. Did you enable internal pull-down or put external pull-down for KBI0 pin1?

Here the "deasserted logic levels" is 0v for your configuration.Edge-only sensitivity.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,766 Views
lmg
Contributor III

Thanks! Very helpful summary.

~LMG

0 Kudos
Reply
1,766 Views
mjbcswitzerland
Specialist V

Hi

See the ARM core documentation, which is not included in the user's manual: http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.dui0662b/Cihbiadi.html

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

0 Kudos
Reply