Hello everyone,
I use K70MCU, CW10.6, USB Stack v4.1.1 and LCD-RGB.
When run the demo "USB Stack->Host->Example->Printer" under CW , it is work fine.
While when i enable the bellow settings for speed up the LCD-RGB display update rate, but USB is not working.
// turn code cache on
LMEM_PCCCR = (LMEM_PCCCR_GO_MASK | LMEM_PCCCR_INVW1_MASK | LMEM_PCCCR_INVW0_MASK | LMEM_PCCCR_ENWRBUF_MASK | LMEM_PCCCR_ENCACHE_MASK);
while( LMEM_PCCCR & LMEM_PCCCR_GO_MASK ){};
// turn system cache on
LMEM_PSCCR = ( LMEM_PSCCR_GO_MASK | LMEM_PSCCR_INVW1_MASK | LMEM_PSCCR_INVW0_MASK | LMEM_PSCCR_ENWRBUF_MASK | LMEM_PSCCR_ENCACHE_MASK);
while( LMEM_PSCCR & LMEM_PSCCR_GO_MASK ){};
// Enable IPF/DPF/IC/DC
FMC_PFB01CR ^= 0x00000001F;
FMC_PFB23CR ^= 0x00000001F;
// Enable IPF/DPF/IC/DC
FMC_PFB01CR |= 0x00000001F;
FMC_PFB23CR |= 0x00000001F;
Is there any settings to handle to speed up the LCD-RGB display update rate with out disturbing K70 USB-Host.
Thanks,
Prabhu.S
Hi PRJOY,
Please tell me where you setting the code in the USB host example code?
I think you can try to configure these code after the USB initialization is OK, and test it again.
Besides, you can configure the interrupt priority, make the USB interrupt priority higher than the LCD update priority.
Wish it helps you!
If you still have question, please contact with me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Jingjing Zhou,
Thanks for the reply.
Now i tried USB-Host Task only with cache on setting and removed display task (LCD-RGB).
I followed your instructions(configure cache on setting code after the USB initialization), still usb (interrupt) is not getting.
Please help me on this
In my application ".data + .bss" section is greater than 128kb, so i mapped ".data + .bss" section into the external DDR memory
/* Specify the memory areas */
MEMORY
{
m_interrupts (rx) : ORIGIN = 0x00000000, LENGTH = 0x1E8
m_cfmprotrom (rx) : ORIGIN = 0x00000400, LENGTH = 0x10
m_text (rx) : ORIGIN = 0x00000800, LENGTH = 1M - 0x800
| m_data | (rwx) : ORIGIN = 0x70000000, LENGTH = 11M | |
| m_data2 | (rwx) : ORIGIN = 0x70B00000, LENGTH = 1M | 
}
Thanks,
Prabhu.S