K70 + Display without VSYNC & HSYNC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K70 + Display without VSYNC & HSYNC

跳至解决方案
972 次查看
joelesco
Contributor III

Hi !

I would like to plug with the Kinetis K70 a display (Winstar WF43G)  wich do not have VSYNC and HSYNC ! It only need the pixel clock. I'm using the D4D with CW. I would like to modify the low_level_drivers.

I was trying first my code with the TWR-LCD-RGB .  The frequency typ. of the LCD CLOCK was  10.87 Mhz, now I would like to change it to 9Mhz.

If someone can guide me for this manipulation would be very nice !!!!!!!!!!


Thanks a lot

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
656 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Not really, the register programming is independent of OS used  or in a bare metal, but it can vary where the register setup is done (PLL, DIVISORS,…etc).

You need to have a look at the LCDC Pixel clock chain:

Most probably your solution is using PLL0 output (SIM_SOPT2) and then going to SIM_CLKDIV3 and then LCDC_LPCR_PCD

So, check what is your PLL0/PLL1 output frequency and calculate LCDCFRAC/LCDCDIV for your required pixel clock.

Check D4DLCDHW_Init_K70LCDC_TwrRgbB(void) function.

LCDC_LPCR_PCD(D4DLCDHWFB_PANEL_CLKDIV);             //Divide 120 PLL clock by (12+1)=13 to get 9.23MHz clock

And for your display, I am not sure if you need to specify the Vertical and blanking periods back porch, front porch,..etc. You will have to check the display datasheet.

Luis

在原帖中查看解决方案

0 项奖励
回复
4 回复数
656 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Are you using MQX?

Regards,

Luis

0 项奖励
回复
656 次查看
joelesco
Contributor III

Hello Luis,

For the moment i'm using Baremetal only. Does that change something ?

Thanks !

0 项奖励
回复
657 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

Not really, the register programming is independent of OS used  or in a bare metal, but it can vary where the register setup is done (PLL, DIVISORS,…etc).

You need to have a look at the LCDC Pixel clock chain:

Most probably your solution is using PLL0 output (SIM_SOPT2) and then going to SIM_CLKDIV3 and then LCDC_LPCR_PCD

So, check what is your PLL0/PLL1 output frequency and calculate LCDCFRAC/LCDCDIV for your required pixel clock.

Check D4DLCDHW_Init_K70LCDC_TwrRgbB(void) function.

LCDC_LPCR_PCD(D4DLCDHWFB_PANEL_CLKDIV);             //Divide 120 PLL clock by (12+1)=13 to get 9.23MHz clock

And for your display, I am not sure if you need to specify the Vertical and blanking periods back porch, front porch,..etc. You will have to check the display datasheet.

Luis

0 项奖励
回复
656 次查看
joelesco
Contributor III

Thanks a lot Luis for your help and all the details  !

0 项奖励
回复