K66F AKU242 MIC1 levels are really low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K66F AKU242 MIC1 levels are really low

2,169 Views
aaronminner
Contributor III

I'm writing an application that uses the AKU242 on-board microphone to process ambient sound.  However, the input is really low.  During testing, it really only records tapping directly on top of it.  Is it a gain issue?  I see defines for gain values - such as kDA7212_DACGain12DB - but it appears they're used only for playback, not input.  Here's the relevant code, mostly taken from the SDK provided example source:

format.bitWidth = kSAI_WordWidth16bits; // kSAI_WordWidth8bits; // kSAI_WordWidth32bits;
 format.channel = 0U;
format.sampleRate_Hz = kSAI_SampleRate32KHz;
#if (defined FSL_FEATURE_SAI_HAS_MCLKDIV_REGISTER && FSL_FEATURE_SAI_HAS_MCLKDIV_REGISTER) || \
 (defined FSL_FEATURE_PCC_HAS_SAI_DIVIDER && FSL_FEATURE_PCC_HAS_SAI_DIVIDER)
 format.masterClockHz = OVER_SAMPLE_RATE * format.sampleRate_Hz;
#else
 format.masterClockHz = SAI_CLK_FREQ;
#endif
 format.protocol = config.protocol;
 format.stereo = kSAI_Stereo;
 format.isFrameSyncCompact = true;
#if defined(FSL_FEATURE_SAI_FIFO_COUNT) && (FSL_FEATURE_SAI_FIFO_COUNT > 1)
 format.watermark = FSL_FEATURE_SAI_FIFO_COUNT / 2U;
#endif

CODEC_Init( &codecHandle, &boardCodecConfig );
CODEC_SetFormat( &codecHandle, format.masterClockHz, format.sampleRate_Hz, format.bitWidth );

DA7212_ChangeInput( &codecHandle, kDA7212_Input_MIC1_An );

The same code works fine if I use the AUX input channel with line level values.  So, by process of elimination, I lean toward some issue with the AKU242.

Labels (1)
Tags (1)
0 Kudos
Reply
5 Replies

2,027 Views
aaronminner
Contributor III

Follow-up: Turns out I somehow broke the on-board MEMS mic on this K66F board.  The SAI demo code to which you referred *did* work, and the code I had been using also worked with a minor tweak, on the new K66F I got.  I tried both programs on the old K66F and they didn't work at all, using the on-board mic, though the AUX input works.  Something I did with the older board must have damaged the circuitry. So, at least I know why the MIC1_Dig input isn't working on my original K66F.  Thanks for the assistance, Felipe!

0 Kudos
Reply

2,027 Views
FelipeGarcia
NXP Employee
NXP Employee

Your welcome! Thanks for keeping the post updated.

 

Best regards,

Felipe

0 Kudos
Reply

2,027 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Aaron,

 

I have used the MIC on my side and I did not perceive the levels low as your description I was able to hear ambient sound through the headphone jack.

 

For your reference, I used the frdmk66f_sai example from the SDK. I modified the example to use the digital microphone by defining DIG_MIC on the project.

 

I used FRDM-K66F, SDK 2.7.0 and MCUXpresso IDE 11.1.1 for my tests. Please let me know your inputs.

 

Best regards,

Felipe

0 Kudos
Reply

2,027 Views
aaronminner
Contributor III

I created a new project with the K66F 2.7 SDK and used the sample code as a base.  The output of both AUX and Mic1 are almost inaudible.  I even went back to my earlier project with SDK 2.5, which had sort-of worked with AUX, but not really with Mic1, and the audio, there, was also nearly inaudible.  I think the board has been damaged, so I ordered a new one.  For completeness, I'll follow up on this after the new one arrives.

Though, curiously, in the SDK 2.5 project, with my oscilloscope I could see data moving on I2S_RXD / PTE7, but that pin flatlines in the 2.7 SDK.  They must've routed signals differently in the two projects.

0 Kudos
Reply

2,027 Views
aaronminner
Contributor III

Thanks for the feedback, Felipe.  I actually read your earlier related question and used your code as a starting point for some adjustments to mine.  However, my MCUXpresso workspace got corrupted as I was working on a new project to test - dunno what happened; it was working yesterday - so I had to toss the project.  I'll give it another try and let you know.  Thanks again.

0 Kudos
Reply