K66 SPI MISO Decay

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K66 SPI MISO Decay

2,601 次查看
lfost
Contributor III

Working with a k66 micro.  Noticed the spi miso line ends high then drifts low.  The k64 does not do this.  No software affects it.  A pull up resistor fixes the decay/drift but is typically not done.  Is this normal for a k66?

0 项奖励
回复
2 回复数

2,585 次查看
myke_predko
Senior Contributor III

@lfost 

If you're not using one of the SPI pin functions, you don't need to assign a pin to the function.  

That's the easiest solution (with the next easiest one putting a pull up on it or tying the pin to GND the way you have) otherwise you'll probably see delays and other weirdness.  

0 项奖励
回复

2,590 次查看
nxf77486
NXP TechSupport
NXP TechSupport

Hello @lfost ,

 

Some followers leaves the line floating when he is not handling it. In these cases the recommendation is to configure a pull-up in the MISO line so that it does not float when the follower so not driving the line.

0 项奖励
回复