K64Fio口中断执行速度

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K64Fio口中断执行速度

1,453 Views
2783828134
Contributor II

求助各位坛友,大家熟悉K64F里的io口速度(就是io口中断执行的的速度)吗?我实验发现io口中断响应速度才达到1M,达不到我的要求,我需要达到3M,但我找不到添加io速度配置的函数,大家可以帮忙提个建议吗?

我自己设置PB9上升沿中断,在中断处理函数里面翻转PC7的电平,然后给pB9  方波,再测PC7 io口的波形,发现1.0M以上的频率,PC7的翻转频率500K之后就上不去了。
Labels (1)
4 Replies

1,274 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 方 鹏,

请问你是想获知中断响应速度,还是想测试IO口翻转频率?

你描述的情况应该是IO口翻转速度跟不上中断速度导致的,可以通过中断里计数满10次再翻转验证该原因。


Kinetis K系列的GPIO翻转速度远低于L系列,L系列的FGPIO翻转速度能够更快。(参考全新FAQ-Kinetis系列产品常见问题总结附件文档“10.1 KL25的IO口最高翻转频率”章节内容)


Cortex M4内核的K64中断执行速度参考:A Beginner’s Guide on Interrupt Latency - and Interrupt Latency of the Arm Cortex-M processors

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,274 Views
2783828134
Contributor II

您好!感谢大佬回答。我想测试的是中断响应速度,和中断执行速度。

我在做的是一个音频采集,按照如下时序读取io口输入,在bclk的上升沿读取DOUT:

pastedImage_1.png

LRCOUT是8KHZ,BCLK是2.8MHZ,发现读取不到io口输入,绝大部分的值都是0。我刚试了一下,在中断里计数到20,对输入40分频(排除io翻转速度的问题),发现速度还是只能达到1MHZ。cortex-m4 中断响应12个CLK,主频120MHZ,理论响应速度能达到10MHZ,现在才1MHZ。这个说明中断响应速度还是不够吧?谢谢您!

0 Kudos
Reply

1,274 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

进出中断的时间根据内核类型是固定的,但中断里代码执行时间可能需要用systick实测

systick.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,274 Views
2783828134
Contributor II

感谢您的回答!

你好,我做的是音频采集,按照时序读取io口电平,然后分离各位得到采样值。时序如下:pastedImage_1.png

LRCOUT是8KHZ,BCLK是2.8MHZ,采集到的数据处理过后绝大部分是0,和实际情况不符。这个是由于在中断里面读取io口的速度不够?还是中断来不及响应呢?按理说120MHZ主频处理这些应该够了呀。跪求大佬指点!

0 Kudos
Reply