K60 POR (power-on reset) is it possible to adjust V_por?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K60 POR (power-on reset) is it possible to adjust V_por?

955 次查看
toebs
Contributor I

Hello 

I am using the NXP Kinetis K60 (http://www.nxp.com/assets/documents/data/en/reference-manuals/K60P144M150SF3RM.pdf

Is it possible to adjust the voltage level of the POR? Or is it always fixed at the levels specified by datasheet? 

标记 (4)
0 项奖励
回复
1 回复

760 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

No, Unfortunately this voltage value cannot be modified, it is used to protect MCU to not get damaged when low voltages are detected.

If it works for you, you could use LVD (low voltage detection) system, which has a LVD reset operation, where the low-voltage detection threshold is determined by LVDSC1[LVDV]; you could use LVDL=1.60 or LVDH=2.56.

Hope this information could help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复