K60 POR (power-on reset) is it possible to adjust V_por?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 POR (power-on reset) is it possible to adjust V_por?

963 Views
toebs
Contributor I

Hello 

I am using the NXP Kinetis K60 (http://www.nxp.com/assets/documents/data/en/reference-manuals/K60P144M150SF3RM.pdf

Is it possible to adjust the voltage level of the POR? Or is it always fixed at the levels specified by datasheet? 

0 Kudos
Reply
1 Reply

768 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

No, Unfortunately this voltage value cannot be modified, it is used to protect MCU to not get damaged when low voltages are detected.

If it works for you, you could use LVD (low voltage detection) system, which has a LVD reset operation, where the low-voltage detection threshold is determined by LVDSC1[LVDV]; you could use LVDL=1.60 or LVDH=2.56.

Hope this information could help you.
Have a great day,
Jorge Alcala

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply