K60 Demo available ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 Demo available ?

Jump to solution
2,049 Views
mkrug
Contributor II

Hello,

 

I have justed received the K60 Tower + LCD. It comes with quite nice demos. Are they available in source code or as binary file ? I just want to make sure I can restore the demo after I am writing the first time to the internal flash.

 

Best Regards

Markus

0 Kudos
Reply
1 Solution
1,626 Views
iafg
Contributor IV

Generally all the code that ships with a tower kit can be found by following the www.freescale.com/tower link and selecting the appropriate board from the dropdown menu.

Then look at the documentation or Download tabs.

 

Look at this link, and confirm that the examples you see are included in the KinetisSC section:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512&fpsp=1&tab=Documentation_...

 

TWRK60N512QSDLAB 
TWR-K60N512 Quick Start Demo Software and Lab Guide

 

Other code is available under downloads tab

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512&fpsp=1&tab=Design_Tools_T...

 

Iain Galloway

Field Applications Engineer - Future Electronics

www.futureelectronics.com

 

(Corporate customers of Future Electronics are encouraged to ask for Engineering assistance anywhere in the world we have offices.)

 

View solution in original post

0 Kudos
Reply
3 Replies
1,627 Views
iafg
Contributor IV

Generally all the code that ships with a tower kit can be found by following the www.freescale.com/tower link and selecting the appropriate board from the dropdown menu.

Then look at the documentation or Download tabs.

 

Look at this link, and confirm that the examples you see are included in the KinetisSC section:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512&fpsp=1&tab=Documentation_...

 

TWRK60N512QSDLAB 
TWR-K60N512 Quick Start Demo Software and Lab Guide

 

Other code is available under downloads tab

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60N512&fpsp=1&tab=Design_Tools_T...

 

Iain Galloway

Field Applications Engineer - Future Electronics

www.futureelectronics.com

 

(Corporate customers of Future Electronics are encouraged to ask for Engineering assistance anywhere in the world we have offices.)

 

0 Kudos
Reply
1,626 Views
mkrug
Contributor II

Hello Iain,

 

it seems to me that the file:

 

TWRK60N512QSDLAB 
TWR-K60N512 Quick Start Demo Software and Lab Guide

 

is broken. While self-extracting it say's that: Error occurred when extracting the twr-k60n512_quick_start_demo.cspy.bat file.

 

I have the LCD module for the Tower Kit. Does the quick start demo software also include the demo application that is shown on the screen after power up ?

 

Best Regards

Markus

0 Kudos
Reply
1,626 Views
mkrug
Contributor II

Sorry, everything fine if you extract the file as an Administrator.

 

Best Regards

markus

0 Kudos
Reply