K60 ADC's value read problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K60 ADC's value read problem

2,469 次查看
kkkk
Contributor II

I enable ADC1_DP1 & ADC2_DP0. I get the ADC key value by my code successfully. But I don't know how to enable multi-ADC pins, such as ADC1_DP1,ADC1_DP3,ADC1_SE18,ADC1_SE23. How do I get each single ADC pin value? Here is my code. Thanks a lot.

void api_ADC_Init(void)

{

  SIM_SCGC3 |= SIM_SCGC3_ADC1_MASK;

  ADC1_SC3 |= 0x80;//ADC1 self-calibration

  while(ADC1_SC3&0x80)

  _time_delay(100);

  ADC1_CFG1 = ADC_CFG1_ADICLK(0) | ADC_CFG1_ADIV(1) | ADC_CFG1_MODE(2);

  ADC1_SC2 = 0x00;

  ADC1_SC1A = 0x41;//ADC1_DP1

  SIM_SCGC6 |= SIM_SCGC6_ADC2_MASK;

  ADC2_SC3 |= 0x80;//ADC2 self-calibration

  while(ADC2_SC3&0x80)

  _time_delay(100);

  ADC2_CFG1 = ADC_CFG1_ADICLK(0) | ADC_CFG1_ADIV(1) | ADC_CFG1_MODE(2);

  ADC2_SC2 = 0x00;

  ADC2_SC1A = 0x40;//ADC2_DP0

}

SystemStatus api_GetADCValue(api_ADCChannel_t B_ADCChennel, WORD *Wp_ADCValue)

{

SelectADCConvertChannel((api_ADCChannel_t) B_ADCChennel);

  cl_ForceDelay_us(15);

  if ((B_ADCChennel == api_ADC_CH1)&&(ADC1_SC1A&ADC_SC1_COCO_MASK ))

  {

  *Wp_ADCValue = ADC1_RA;

  ADC1_SC1A = 0x41;//initiate a new conversion

  return OK;

  }

  if ((B_ADCChennel == api_ADC_CH2)&&(ADC2_SC1A&ADC_SC2_COCO_MASK ))

  {

  *Wp_ADCValue = ADC2_RA;

  ADC2_SC1A = 0x40;//initiate a new conversion

  return OK;

  }

  cl_ForceDelay_us(1);

  return NO_DATA;

}

标签 (1)
标记 (2)
0 项奖励
回复
5 回复数

1,798 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

It need to modify ADC Status and Control Registers 1 (ADCx_SC1n) [ADCH] bits to select the input ADC channel.

There is another way, which using DMA to help ADC do a scan work (multi channels can be sampled and conversion), more detailed info, please check below link:

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf


Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,798 次查看
samz
Contributor I

Generally, it trigger the ADC conversion, then check the status, read the ADC register when it finish conversion.


I use processor expert to generate ADC code, it seems not make sense.

The PE setting for ADC are:

                 Discontinuous Mode    ===>yes

                 Static sample groups   ===>Enabled

After generating code, it only have three function:

                  Init                             - LDD_TDeviceData* ADC_InputPS_Init(LDD_TUserData *UserDataPtr);

                  CreateSampleGroup - LDD_TError ADC_InputPS_CreateSampleGroup(LDD_TDeviceData *DeviceDataPtr,...

                 GetMeasuredValues -  LDD_TError ADC_InputPS_GetMeasuredValues(LDD_TDeviceData *DeviceDataPtr,...

   ===========================================================================================

I can't find how to use CreateSampleGroup()   to trigger and check status, is there any example for how to use the ADC?

0 项奖励
回复

1,798 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Sam,

Please let us know which Kinetis product you are using?


Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,798 次查看
samz
Contributor I

The MCU is MK60DX256VLL10.

0 项奖励
回复

1,798 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Sam,

You can download K60 example code from below link:

KINETIS512_V2_SC : Kinetis 100MHz Rev 2 Example Projects.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=K60_100&nodeId=01624698C9DE2DDDAF&fps...

It includes ADC example code.


Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复