K60 ADC eternal sequencing of 12 inputs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 ADC eternal sequencing of 12 inputs

Jump to solution
1,717 Views
michelc
Contributor I

Hi, I have to scan 12 single ended inputs of ADC1 with 8 bits result eternally.

I would like to do this without CPU intervention, so in DMA mode modulo 24, using 2 buffers of 12 bytes.

Is this possible? (cfr. X-Scale Stellaris can)

Thx,

Michel

Labels (1)
0 Kudos
Reply
1 Solution
1,413 Views
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

View solution in original post

0 Kudos
Reply
2 Replies
1,414 Views
ndavies
Contributor V

An application note appeared yesterday that should answer your question.

http://cache.freescale.com/files/32bit/doc/app_note/AN4590.pdf?fpsp=1&WT_TYPE=Application Notes&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=pdf&WT_ASSET=Documentation

0 Kudos
Reply
1,413 Views
michelc
Contributor I

Thanks Norm, that's just what I was looking for!

Michel

0 Kudos
Reply