K40: How to enter into low power modes?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K40: How to enter into low power modes?

跳至解决方案
885 次查看
BasePointer
Contributor II

Hi,

I want to measure K40's power consumption at KwikStik board while it is in various low power modes.

I read about AN4503 but the examples given in the datasheet are not compile-able for me.

Where are the example project files for AN4503? (I use KEIL IDE and C)

Thanks.

标记 (3)
0 项奖励
1 解答
598 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
1 回复
599 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励