K40: How to enter into low power modes?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K40: How to enter into low power modes?

ソリューションへジャンプ
1,705件の閲覧回数
BasePointer
Contributor II

Hi,

I want to measure K40's power consumption at KwikStik board while it is in various low power modes.

I read about AN4503 but the examples given in the datasheet are not compile-able for me.

Where are the example project files for AN4503? (I use KEIL IDE and C)

Thanks.

タグ(3)
0 件の賞賛
返信
1 解決策
1,418件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,419件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信