K32 L2A Force RESETn pin to be dedicated

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32 L2A Force RESETn pin to be dedicated

Jump to solution
595 Views
sachin_patel
Contributor III

Hi,

 

I am using a Kinetis K32 L2A microcontroller in our design. As part of our model, we require the RESETn pin to be dedicated (i.e. it must not be possible from software to change it's pin mux state).

I can see in the Reference Manual Chapter 6.3.2: FTFA_FOPT[3]:

RESET_PIN_CFG: When set to 1, it says the following: "RESET_b pin is dedicated. The port is configured with pullup enabled, open drain, passive filter enabled".

Does this mean that the option to mux the pin as anything other than RESET_b is now disabled?

Thanks,

Sachin Patel

0 Kudos
1 Solution
584 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

View solution in original post

0 Kudos
1 Reply
585 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

0 Kudos