K27F-K28F USB VREG_OUT Capacitor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K27F-K28F USB VREG_OUT Capacitor

1,303 次查看
etronic_arg
Contributor III

Hi,

I just want to know if VREG_OUT (pin G2) should be connected to an external output capacitor (COUT=2.2uF in datasheet) despite of it is not used to power any external circuit. I want to use USB FS with IRC48 as clock source. The microcontroller is powered by an external supply.

Thanks!

标签 (2)
0 项奖励
回复
2 回复数

1,190 次查看
mjbcswitzerland
Specialist V

Hi

The capacitor is used to stabilise the low dropout regulator used to supply stable USB PHY power supply. This means that if FS USB is used it must be connected. If not, USB will not work.
Make sure that the capacitor type used fulfills the low ESD requirements as specified in the manual and data sheet.

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

1,190 次查看
etronic_arg
Contributor III

Thank you. Just as I thought! I didn't realize to put it in my board... 

0 项奖励
回复