K22FN128 FLL reference clock questions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22FN128 FLL reference clock questions

1,432 次查看
isaotakashima
Contributor IV

We will use the MK22FN128 MCU with 20 MHz external crystal, and set core clock to 100 MHz in FEE mode.

I believe that we can set core clock to 100 MHz as below.

- FLL reference clock = 39.0625KHz (= 20 MHz / 512)

- FLL DCO output clock = 39.0625KHz * 2560 = 100MHz.

As you know, the maximum FLL reference frequency range is 39.0625 KHz.

Can I use crystal which 50 ppm frequency tolerance?

Because frequency of crystal is 20 MHz +/- 1 KHz and FLL reference clock is 39.0625 KHz +/- 1.95 Hz, some case exceed 39.0625 KHz.

Then I want to make sure that I can use 50 ppm crystal or not.

Please reply as soon as possible.

Best regards,

Takashima

标签 (1)
0 项奖励
回复
4 回复数

1,238 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Takashima,

I think it's available, however it's necessary to implement stability verification before the manufacturing.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,238 次查看
isaotakashima
Contributor IV

Dear Jeremyzhou,

Thank you for your reply.

I would like to confirm your answer. If you want to say that I should use the crystal which frequency within specification including frequency tolerance, I should use 19.999 MHz 50 ppm crystal or 20 MHz  0 ppm crystal. But I cannot get these parts.

Then I would like NXP to guarantee that I use 20 MHz 50 ppm crystal.

Can NXP do that?

Please reply as soon as possible.

Best regards,

Takashima

0 项奖励
回复

1,238 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Takashima,

The MCU usually has the extend frequency arrange for clock source, so I think you can give a try.

As I stated above, you also need to do some stability verification testing for it.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,238 次查看
isaotakashima
Contributor IV

Dear Jeremyzhou,

Thank you for your reply.

I don't have good test procedure to confirm stability verification testing.

Best regards,

Takashima

0 项奖励
回复