K22F updates using DFU and MCUXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22F updates using DFU and MCUXpresso

3,298 次查看
karamanr
Contributor I

Hello,


The main idea of my project is to update the software OTA using MCUBoot, DFU and Mender. I followed this https://hub.mender.io/t/updating-device-firmware-using-dfu-in-zephyr-project-on-a-frdm-k64f-board/16... to set up MCUBoot and DFU for my board and it all works fine. However, the next step is putting and application build with MCUXpresso on the K22F board. What is the best way to approach this? Do I need to use tools from the Zephyr Project to build my application or is there a tool that I can use with MCUXpresso to build and sign my application?  

0 项奖励
回复
4 回复数

3,254 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @karamanr ,

I think to the application, it needn't any special building. You can use MCUXpresso to build it, put the start address in dedicated space and use the tool in Zephyr to sign the image.

 

Regards,

Jing

0 项奖励
回复

3,179 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Here is a guide. Hope it can be helpful.

 

Regards,

Jing

0 项奖励
回复

3,241 次查看
karamanr
Contributor I

Hi and thanks for your reply,
I have tried using the binary built by MCUXpresso and sign it with the Zephyr tools, however it seems that MCUBoot is unable to detect the image when I flash it to the board using DFU.

0 项奖励
回复

3,266 次查看
D4Worker
Contributor II

We have similar question on KVF46f,  appreciate for any response.

0 项奖励
回复