K22 family observations/feedback

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22 family observations/feedback

2,261 次查看
jrychter
Contributor V

I recently took a first look at the K22 family and I have some observations. I don't know where else to post this, so I'm posting here, hoping it will reach the right people.

I've been looking at migrating from K20 to K22 in a low-cost USB device project. I looked at the K22 family and… well, I'm not happy. Here are my main observations:

  • The K22 is supposed to be "optimized for cost-sensitive applications". Sounds great! I was so happy to see crystal-less USB operation, the crystal is always a significant cost component, both in terms of BOM cost and board space! But then I discovered that the small K22 devices with FP that I wanted to use (MK22FN128) do not have the USB VREG! Why, oh, why? This means that I can save on the crystal, but have to add the cost of an external LDO! Not good! What's even worse is that it's very difficult to find out that the VREG isn't there. There is even a bug in the datasheet: the front page of K22P100M100SF9 says "USB LS/FS OTG 2.0 with embedded 3.3 V, 120 mA LDO voltage regulator", which is not true. Only the KINETISKMCUSELGD shows the lack of integrated LDO if you look closely (the lack of a (2) footnote next to four devices). Why was the VREG removed from those 4 devices? It makes no sense.
  • Packaging. The entire K22 family doesn't have a single QFN device. It's a disaster for people designing small cost-sensitive devices: you can't use BGA because of the PCB requirements increasing costs significantly, so you're stuck with the huge LQFP packages. The smallest I can use is 64LQFP, which is 10x10mm, while right now I'm at 32QFN (5x5mm) with the K20.

The K22 devices would be perfect for my applications if it wasn't for the above problems.

标签 (1)
标记 (3)
0 项奖励
回复
3 回复数

1,965 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Jan

K22 has IRC48M inside for USB module, so you need to add external clock for USB. I think this will cost down your application.

You can find more package from link K22_50 |Kinetis K22 50 MHz MCUs|Freescale

Hope my reply can help you.

Best Regards

Paul

0 项奖励
回复

1,965 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Jan

This device is cheaper and also give you a chance to select a matched LDO. For example, there is no many IC used 3.3V, then you can select lower current output LDO. Standing on PCB size point, LDO area is almost the same as oscillator/crystal. Standing on BOM cost point, new MCU+LDO is cheaper than old MCU+oscillator/crystal.

Hope my reply can help your understanding our design. Thanks.

Best Regards

Paul

0 项奖励
回复

1,965 次查看
jrychter
Contributor V

Was the VREG really a significant cost factor? Will I really see it reflected in the device prices? Will the no-VREG devices+LDO really be cheaper than a VREG-included device? I am not convinced here. Perhaps we will see this over time, as all K22 devices get introduced and make their way to distributors.

Also, what about the packaging? WLCSP/BGA means expensive PCBs. No QFN means no cheap and small 2-layer boards/products.

0 项奖励
回复