K10 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K10 board

1,215 次查看
Bolt
Contributor I

Does anyone know a board with the k10 of 48 pins?

Thanks in advance

标签 (1)
标记 (1)
0 项奖励
回复
3 回复数

1,115 次查看
LuisCasado
NXP Employee
NXP Employee

Hi Javi,

What do you mean? A third party board using the K10 in 48 pins to buy as finished board?

Best Regards,

Luis

0 项奖励
回复

1,115 次查看
Bolt
Contributor I

Hi Luis,

No, it's just to go doing the software for the same part as in our project.

Thanks

0 项奖励
回复

1,115 次查看
LuisCasado
NXP Employee
NXP Employee

Hi Javi,

Ok, I don't know any board with K10, I am not sure about what K10 you need (50, 72, 100 Mhz,...) But the code you write at the same speed grade Kinetis (K60, K20,..) will be 100% compatible if you use the same peripherals that K10 has. But the GPIOMUX will have to be tuned for your custom harware with K10.

Perhaps anyone knows in the community about an available board.

Luis,

0 项奖励
回复