JTAG connections

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JTAG connections

2,891件の閲覧回数
pasini
Contributor I

We are using MK22FN1M0VLQ12 . What are the minimum signals needed for JTAG connection ?

We plan to use PEMICRO Multilink Universal ( 20-pin connector ). Where can I find this information ?

Thanks in advance,

Luiz

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,647件の閲覧回数
dave408
Senior Contributor II

Luiz, I use a Segger J-Link with the K22F and K64F which also has a 20pin connector.  However, there is a 10pin Cortex-M adapter that plugs into the hardware and then has a 10pin ribbon connection.  So you likely really only need these connections.

pastedImage_0.png

0 件の賞賛
返信

2,646件の閲覧回数
thomaskang-b295
NXP Employee
NXP Employee

Hello Luiz,

K22 has several debug interfaces as below. For minimum debug signals, SWD is recommended unless JTAG is mendatody.

Debug.JPG

For your use of Multilink Universal, the attachement can help. Please look into connector chapter then you can find info.

Connections 1.JPG

Connections 2.JPG

Thank you,

Thomas Kang

0 件の賞賛
返信

2,646件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Luiz,

Please check Kinetis K family product debug interface at chapter 2.1.5.3 of <<Kinetis Peripheral Module Quick Reference>>

It also could refer K22 product JTAG debugger circuit of TWR-K22F120M board schematics.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信