Hi Isaac Romero,
What the VLLS mode you are using? If you are using VLLS1/3, you can use the LPTMR with 1khz LPO as the wake up source to make the VLLS1/3 more than 1minute.
You can choose LPO as LPTMR clock source.



Then, from the LPTMR register:

CMR is 16 bit, it is 65536, so you can reach:65536*1ms=65.536s intervals.
so you can reach 60s =1minute.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------